Normally, Keysight power supplies are delivered configured to deliver their full specs at the output terminals. In some application, where long lead lengths to the DUT are unavoidable, the regulation of the power supply at the DUT can be significantly improved by using remote sensing. The sense leads effectively connect the inputs to the power supply control loop directly to the DUT. Since there is negligible current in these sense leads, the exact voltage at the DUT is communicated back to the power supply. Now any resistance in the load leads is essentially brought inside the power supply control loop, and is effectively "eliminated"?
The amount of drop in the load leads that the sense leads can correct for is limited. In general, most Keysight dc power supplies can handle up to 2 volts in each load lead. Some power supplies are available which can drop up to half the rated output in each lead. Of course, the total drop in the load leads subtracts from the rated voltage available for the DUT. For more detailed information on remote sensing specifications,see Keysight Power Supplies and Electronic Loads.
Applies to: All models
Visit our Power Products Forum for additional topics and discussions. Read technical postings on our Power Blog – Watt’s Up? |
6030A, 6031A, 6032A, 6033A, 6035A, 6038A, 6060B, 6063B, 6621A, 6622A, 6623A, 6624A, 6625A, 6626A, 6627A, 6628A, 6629A, 6641A, 6642A, 6643A, 6644A, 6645A, 6651A, 6652A, 6653A, 6654A, 6655A, 6671A, 6672A, 6673A, 6674A, 6675A, 6680A, 6681A, 6682A, 6683A, 6684A, 6690A, 6691A, 6692A, E4356A, 6611C, 6612C, 6613C, 6614C, 6631B, 6632B, 6633B, 6634B, 66309B, 66311B, 66312A, 66319B, 66319D, 66321B, 66321D, 66332A, 66000A, 66001A, 66002A, 66101A, 66102A, 66103A, 66104A, 66105A, 66106A, 6811B, 6812B, 6813B, AC6801A, AC6802A, AC6803A, AC6804A, E4360A, E4361A, E4362A, E4366A, E4367A, E4368A, E3620A, E3630A, E3631A, E3632A, E3633A, E3634A, E3640A, E3641A, E3642A, E3643A, E3644A, E3645A, E3646A, E3647A, E3648A, E3649A, E36102A, E36103A, E36104A, E36105A, E36106A, N3300A, N3301A, N3302A, N3303A, N3304A, N3305A, N3306A, N3307A, N5740A, N5741A, N5742A, N5743A, N5744A, N5745A, N5746A, N5747A, N5748A, N5749A, N5750A, N5751A, N5752A, N5761A, N5762A, N5763A, N5764A, N5765A, N5766A, N5767A, N5768A, N5769A, N5770A, N5771A, N5772A, N6700B, N6701A, N6702A, N6705A, N6705B, N6710B, N6711A, N6712A, N6715A, N6715B, N6731B, N6732B, N6733B, N6734B, N6735B, N6736B, N6741B, N6742B, N6743B, N6744B, N6745B, N6746B, N6773A, N6774A, N6775A, N6776A, N6777A, N6751A, N6752A, N6753A, N6754A, N6755A, N6756A, N6761A, N6762A, N6763A, N6764A, N6765A, N6766A, N6781A, N6782A, N6785A, N6786A, N6783A-MFG, N6783A-BDA, N6784A, N6950A, N6951A, N6952A, N6953A, N6954A, N6970A, N6971A, N6972A, N6973A, N6974A,N6976A, N6977A, N7950A, N7951A, N7952A, N7953A, N7954A, N7970A, N7971A, N7972A, N7973A, N7974A, N7976A, N7977A, N8731A, N8732A, N8733A, N8734A, N8735A, N8736A, N8737A, N8738A, N8739A, N8740A, N8741A, N8742A, N8754A, N8755A, N8756A, N8757A, N8758A, N8759A, N8760A, N8761A, N8762A, N8920A, N8921A, N8923A, N8924A, N8925A, N8926A, N8928A, N8929A, N8930A, N8931A, N8932A, N8934A, N8935A, N8937A, N8937APV, N8940A, N8941A, N8943A, N8944A, N8945A, N8946A, N8948A, N8949A, N8950A, N8951A, N8952A, N8954A, N8955A, N8957A, N8957APV, PA2201A, U8001A, U8002A, U8031A, U8032A